Kit composition - Johnson Controls - LIT-12014122 - OpenBlue - OpenBlue Healthy Buildings

OpenBlue Indoor Air Quality Audit Service Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Healthy Buildings
Document number
LIT-12014122
Revision date
2023-01-17
Product status
Active
  • 24 RESET™ approved IAQ sensors measuring:
    • Temperature
    • RH
    • Carbon dioxide
    • Particulate matter 2.5 µm
    • Particulate matter 10 µm
    • TVOC
    Figure 1. IAQ sensor

  • 3 Cellular Hubs for data communication:

    The IAQ sensors communicate to hubs based on sub-G local network technology. The hubs connect to the cloud through cellular communication and are independent from site IT infrastructure.

    Figure 2. Cellular hub

  • Two particulate matter monitors which measure:
    • Temperature
    • RH
    • Particulate matter in 10 different bin sizes from 0.3 µm to 40 µm
    Figure 3. Particulate matter monitoring sensor

These devices have an embedded cellular communication gateway and are independent from site IT infrastructure.

The first particulate matter monitor is placed outside to measure outdoor particulate such as pollen and fire smoke. 90% of indoor air quality issues originate from outside.

The second particulate matter monitor is placed inside and used in parallel with the indoor IAQ sensors.