Enhancements - Johnson Controls - LIT-12013755 - Software Application - OpenBlue Enterprise Manager - 4.7.2

OpenBlue Enterprise Manager Release Notes

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Release Notes
Document number
LIT-12013755
Version
4.7.2
Revision date
2024-05-15
Table 1. Energy Efficiency and Sustainability enhancements
Package Module Details Benefit
Net Zero Advisor Energy Manager

Auto Sync source utility bills data with matching offline meters

Net Zero Advisor customers use monthly utility bill data rather than interval meter data. For NZA users, Auto Sync continuously matches utility bill data to the corresponding offline meters for the Energy Manager widgets. Whether the updates are manual or automatic, the paired offline meters in Energy Manager now always display the latest utility bill data. Every entry or modification to utility bill data is automatically reflected in the corresponding offline meters' data.

A synchronization between utility bill data and the corresponding offline meters by which that utility bill data is displayed in the Energy Manager page ensures consistency across locations in OBEM and the accuracy of data presented to the user.
Table 2. Space, Wellbeing, and Productivity enhancements
Package Module Details Benefit
Workplace Advisor - Space Space Performance

Improved dashboard layouts

Space Graphics and 3D Viewer have their tab on the floor dashboard. Max occupant widgets on the floor, zone, and room dashboards are in a more prominent position on those dashboards.

Space Graphics playback displays the playback time by default when running playbacks.

Row numbers are added to the Room Comparison report.

  • Users can access the key widgets quicker
  • Analyze the insights that display in the Room Comparison report
  • Space Graphics playback is more efficient
Workplace Advisor Indoor Air Quality Space Performance

Increase in the range of data that displays for Clean Air Delivery, IAQ scores, and IAQ parameters

Increased range of data displays for the Clean Air Delivery score, IAQ score, and IAQ parameters, for example, three months, six months, and one year, compared to current last 30 days data.

More data helps to visualize the impact of seasonal trends and its impact on the occupants through the Indoor Air Quality and Clean Air Delivery data.

Improvements in the IAQ Trend Chart

UX improvement in the IAQ trend chart to preselect the sensors to show graphs of the sensors selected.

Users do not need to click additionally and wait for the data to load. Less clicks lead to better user experience.
Workplace Advisor Indoor Air Quality  

Airthings Integration

OBEM now supports Connectivity with AirthingsĀ® IAQ sensor.

Customers who have Airthings sensors installed can directly connect to OBEM and derive value by tracking IAQ data for occupant comfort and productivity.
Table 3. Operational Efficiency and Equipment Performance enhancements
Package Module Details Benefit
Equipment Performance Advisor Plus Asset Manager

3D Viewer Performance Optimization

This update adds improvements to optimize the Viewer page loading time performance.

Users now experience the loading time reduced by around 5 to 8 seconds. This improves the overall user experience.
Equipment Performance Advisor Reports

Enhance report sharing capability

A new tab, Shared Reports, is available under the Reports section. Previously, users could share the reports from the Saved Reports tab using the notify option. This functionality provides the ability to share the reports from a separate shared reports tab.

Users can view the shared report details under the tab, and from the list section can view the report using filters such as shared last, shared by, and shared to.

A Site admin can disable (temporarily pause) the sharing of the report, so users do not receive unwanted notifications.

  • Users can now view who shared the report and with whom and the site
  • The site admin can disable the sharing of the report, so users do not receive unwanted notifications.
Equipment Performance Advisor and Equipment Performance Advisor Plus Report

FDD Fault Summary Report

This report is for Johnson Controls internal purposes only.

Authorized Johnson Controls internal users can view details of faults triggered across all customers. Users can also identify which of the faults triggered are high-impact rules.

Users can use the fault information to identify and prioritize the fault rules that can be considered for enabling autonomous command actions.

Authorized Johnson Controls internal users can get a list of prioritized high-impact rules that can be considered for enabling autonomous command actions. This allows customer success teams to target ways to deliver more value to our customers.