| Package | Module | Details | Benefit |
|---|---|---|---|
| Net Zero Advisor | Energy Manager |
Default timeframe selections for NZA users Net Zero Advisor OBEM portfolios use monthly utility bill data rather than continuous meter data. For OBEM NZA subscription users, the default timeframes for widgets on both the OBEM landing page and Energy Manager pages default to an annual timeframe to minimize blank widgets and better represent the data availability from monthly utility bills. |
Improves user experience by minimizing the number of blank widgets and providing data-rich visualizations, even if utility bill data for the most the current month has not yet been delivered by the customer’s utility provider. |
| Net Zero Advisor and Net Zero Advisor Plus | Setup |
Meter-level utility data ingestion OBEM ingests utility data from partners such as Arcadia Utility Cloud API to support complex utility bill structures, such as when invoices contain accounts, sub-accounts, and meters for multiple sites. Users can accurately distribute multiple meters loads and line items to a particular building. |
|
| Net Zero Advisor and Net Zero Advisor Plus | Setup |
Invoice copy download Users can view and download copies of utility bills in PDF format, imported from Arcadia, directly from the Setup application’s Utility Bill Manager tab. OBEM provides secure storage of PDF links and retrieval functionality. Note: Copies of manually uploaded invoices are not
currently available for download.
|
|
| Net Zero Advisor and Net Zero Advisor Plus | Energy Manager |
Offline energy meter logic to update timestamp to match utility bill period The improved meter logic processing ensures offline meters that display data in Energy Manager match the utility invoice bill periods. The enhancement addresses unique situations where invoices cross over into multiple months. |
The feature aligns the meter and invoice time period logic to make sure the distribution of utility usage and cost data by month matches between Energy Manager and Utility Bill Manager. |
| Net Zero Advisor Plus | Reports |
Building Solar Energy standard report For Net Zero Advisor Plus users with solar photovoltaic energy production meters, OBEM now offers a standard ReportBuilder PowerBI report option to summarize solar energy generation across the building portfolio in comparison to total building energy use, grid import, and major end-use energy types. The report uses meter type or meter tags to analyze data. |
|
| Package | Module | Details | Benefit |
|---|---|---|---|
| Workplace Advisor Space | Space Performance |
Improvement in the calculation of Maximum Occupancy Improved maximum occupancy calculations across all space levels correctly represent maximum occupancy at higher space levels. This update ensures the occupant reporting at higher space levels does not double count people seen at lower space levels. |
The improved calculation allows users to correlate basic raw data and calculated aggregated data, assuring the correctness of values displayed in the widgets. |
| Workplace Advisor Indoor Air Quality | Space Performance |
Date and Time Indication on IAQ and Clean Air Delivery Score Users can now see the date and time (wherever applicable) on the IAQ scores and Clean Air Delivery scores (time not applicable) and the air quality parameters. |
This helps users to understand when the score was last updated and helps correlate the impact of parameters on the IAQ score. |
|
Improvements in the IAQ alerts section Low Indoor Air Quality Alerts is renamed to Indoor Air Quality by Score. This section contains all the zones that have IAQ scores and the parameters contributing to the IAQ score. When users click on the parameter, they can see the complete details of the parameters, its value, and whether they are in the good, moderate, poor, or hazardous range. |
Users can now view all the zones, its IAQ scores and the parameters contributing to the IAQ scores without having to click through all the zones and get a bird's eye view of all zones in the buildings. | ||
| Workplace Advisor Indoor Air Quality | Space Performance |
View the thresholds for each air quality parameter Users can now see the thresholds associated with each parameter for each zone. |
This is helpful to understand the reason for showing parameters as good, moderate, poor, or hazardous and helps correlate the parameter indication with the thresholds. |
| Workplace Advisor Indoor Air Quality and Performance Advisor | Space Performance |
Introduction of hazardous range in IAQ OBEM adds a fourth category called Hazardous to the IAQ score in categories. |
Users can now see the IAQ score in more detail and its direct impact on health. |
| Package | Module | Details | Benefit |
|---|---|---|---|
| Equipment Performance Advisor and Equipment Performance Advisor Plus | Asset Manager |
Configuration and display of Emergency exit lighting with timestamp points
|
Users can view operational information with respect to the timestamp-related data sets for equipment like emergency exit lighting for example, last discharge test, last function test. This helps to track the health of assets and need for service, maintenance, or replacement. |
| Equipment Performance Advisor | Asset Manager |
Room-level Asset Operational Schedules
|
Users can create a dedicated operational schedule across assets mapped for individual rooms. Facility managers can better tailor fault detection and asset control commands based on a room-specific schedule. |
| Equipment Performance Advisor Plus | Asset Manager |
Display equipment name in header within 3D Viewer Users can now view the name of the selected equipment on the header section of the 3D Viewer to enhance the user experience and avoid repeated equipment names. |
Enhanced user readability and better user experience. |
| Equipment Performance Advisor Plus | Space Performance |
3D Viewer Heatmap View color assignment for IAQ data that exceeds or falls below a threshold
|
Users can now view dedicated colors for values that exceed or fall below thresholds. Previously, when values exceeded or fell below the threshold, the heatmap did not display. This enhancement improves the user experience. |
| Equipment Performance Advisor Plus | Asset Manager |
Equipment name hyperlink The equipment name on the asset KPI cards is a hyperlink to redirect the user to the equipment dashboard for equipment specific information. |
Ease of navigation and quick access to equipment information. |
| Equipment Performance Advisor Plus | Asset Manager |
Run Hours display enhancement Run Hours calculation or elapsed active time is now rounded to the nearest hour while other units are rounded to two decimal places in both the Operation Overview and Define Dashboard pages. |
Users have an improved user experience. |
| Equipment Performance Advisor | Setup |
New equipment type template for Air Handling Unit with Heat Recovery Wheel (Europe region request)
|
Air handling units with heat recovery wheels are common in Europe and other global markets. Users can now use a new AHU Equipment type for this type of HVAC asset. |
| Equipment Performance Advisor and Equipment Performance Advisor Plus | Asset Manager |
Health score definition explanations
|
Users can now better understand what each health score means in the Fault Management page. |
| Equipment Performance Advisor and Equipment Performance Advisor Plus | Multiple |
24K NUS – CMMS Connector
|
OBEM supports a new CMMS connector integration with 24K CMMS system |