Use the Space Tree feature to create a space hierarchy that reflects actual physical locations in the portfolio. The following levels are available in the space hierarchy:
- Portfolio
- Location
- Building
The admin can use space re-ordering to setup the space hierarchy to reflect how the user wishes to view the spaces.
You have the flexibility to add spaces, for example, floor, wing, and rooms below the building level. You can name each one for your personal requirements to provide to provide ultimate flexibility.
The accurate creation of the space tree is critical to the functioning of the OBEM system. Set up the tree to exactly mirror the physical portfolio to allow the energy analysis to be accurate and precise.