Floor based heat maps for IAQ and occupancy - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

The Space Graphics dashboard supports data visualization in the form of KPI labels and heat maps. You can create heat maps and overlay the map onto a floor plan. This provides you with a good indication of how the occupancy or the space IAQ changes over a period of time.

Assign ranges and colors to a single point or template, or to all the points in a template with a single click. Use the time lapse feature to view changes in values in the space over a user-defined time range.

Configured data points from Space Performance and Asset Manager are available to build layers of IAQ and Occupancy information into the Space Graphics widget.