Emissions factors - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

OBEM provides pre-configured emission factors based on the geographic location of the facility and building.

Use the library of emissions factors based on location and utility source to do the following:

  • Calculate and analyze your emissions footprint without sourcing the latest regulatory updates
  • Modify the default emission factor set in Net Zero Advisor
  • Update emissions factors and reprocess underlying data
  • Provide an audit trail of emission factor history and source providers
  • Libraries are available for the United States, Canada, and Europe