OBEM provides pre-configured emission factors based on the geographic location of the facility and building.
Use the library of emissions factors based on location and utility source to do the following:
- Calculate and analyze your emissions footprint without sourcing the latest regulatory updates
- Modify the default emission factor set in Net Zero Advisor
- Update emissions factors and reprocess underlying data
- Provide an audit trail of emission factor history and source providers
- Libraries are available for the United States, Canada, and Europe