Utility Provider Integration - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

OBEM can receive monthly utility bill data through utility providers to fill dashboards in Utility Bill Manager.

OBEM can also receive daily utility bill data from utility providers to fill dashboards in Energy Manager with hourly consumption information. The OBEM team registers the customer information with utility providers, and verifies the successful set up of the automated process. After the setup is complete, the account information is automatically created in OBEM. Meters are automatically created and data points are mapped depending on the information the OBEM team receives. OBEM starts to receive utility bill information and data flows into OBEM.