Support for custom units - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

OBEM supports custom units through offline and virtual meters.

This feature helps you to create unique KPIs such as kWh/Occupant Count to measure the amount of electricity per occupant or other creative KPI.

Additionally, the offline meters support entered values to represent a count, state, or limit.

The data with custom units is available at the respective meter level dashboards and custom dashboards.