Support for commodities - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12
Energy Manager supports the following commodities:
  • Chilled water
  • Coal
  • Compressed air
  • Diesel
  • Electricity
  • Fuel oil
  • High temperature hot water
  • Hot water
  • Liquid propane
  • Natural gas
  • Sewage
  • Steam
  • Waste

OBEM supports these commodities through online, offline, and virtual meters.

Use the meter level and space level dashboards available in Energy Manager to monitor the commodities.