Energy tracker with baseline - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Product Bulletin
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

The Energy Consumption Tracker is available at Portfolio, Location or Building level and is used to show the consumption of all commodities. You can view consumption data for commodities either in chart or tabular format. The tracker shows the consumption of all commodities for the current month. Configure the summary chart to show data by week, by month, 3 months, 6 months or by year and export the data as an SVG, PNG, JPEG image or as a PDF file.

This KPI gives you quick access to compare the Consumption and Demand, demand only for electricity, against the target baseline. It provides the ability to define a Baseline across Commodities, Electricity, Natural Gas, Hot water, and Chilled Water, at both space and meter level, and displays the information in an easy-to-understand graphical representation of difference from the target baseline.