Energy Fault Detection and Diagnostics - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Product Bulletin
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12
OBEM Energy Fault Detection and Diagnostics (FDD) contains the following options to monitor energy:
  • High unoccupied consumption
  • Weekend consumption
  • High energy consumption
  • High occupied energy consumption
  • High unoccupied energy consumption
  • High weekend energy consumption
  • Electrical peak demand above threshold
  • Unoccupied peak demand above threshold
  • Weekend electrical peak demand above threshold
  • Meter Flatline Value Detection
  • Meter Offline Detection
You can view fault data at varying levels, such as by portfolio, location, building, floor, wing, room, or meter.

You can setup automated work order creation for all new and existing energy fault rules.