Alarm Manager - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Product Bulletin
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

Use Alarm Manager to view alarms easily and effectively. Alarm Manager categorizes alarms are by source, priority, and time of occurrence which makes it easier to track all alarms for the entire platform. The alarm manager is not limited to showing alarms on the common dashboard, it is also used as an in-built notification mechanism for alarms to be delivered through SMS and Email. The effective notification feature helps track who, and when, the alarm was delivered through the platform. Configurations are flexible through subscriptions to the necessary notifications.

OBEM supports ingestion of alarm data through data collection devices and from OBB and OBC using BACnet/IP intrinsic communication protocols.

The following additional features are discussed in further detail in the Overview of Alarm Manager features:
  • Alarm analytics
  • Alarm manager widgets
  • Accessibility
  • Localization