Meters and equipment - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

You can add in Meters or Equipment points, including the following tasks:

  • Add and Edit the attributes of data source points
  • Historical Fetch and Sync
  • Create meters and submeters and map the points
  • Assign meter tags to meters for unique references in Report Builder

Online and virtual meters are represented by unique icons that help you to distinguish different types of meters. Meters can include commodities such as electricity, natural gas, water, and steam. Users can add Offline meters, Virtual meters, and points under the Meter configuration tab in the Setup. Users can upload the offline data for the offline meters in the Offline points tab in the Mapped points section of the Setup. Equipment setup can include categories such as chillers, air handling units, boilers, pumps, and fans that users can monitor for performance.