Net Zero Advisor Plus - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12
Net Zero Advisor Plus offers all the benefits of the Net Zero Advisor package and the following features:
  • Automatically collects, analyzes, and displays information for all configured physical meters, online and offline
  • Supports the creation of virtual meters to substitute sub-metering or create calculated values online
  • Consumption and demand comparisons, energy profiling, consumption profiling, and demand profiling

Interval data analysis

Gain insights into your building’s energy consumption patterns and identify areas where you can reduce energy usage.

Determine if the building is turning on at the expected time each day or if the lights and other building systems are setting back as expected each evening and on weekends.

Identify demand spikes that could result in increased costs through ratchet or other tariff-related penalties.

Sub-metering and space level analysis

Monitoring sub-metering is an essential component of energy management. With sub-metering you can track the energy consumption of individual systems or devices, and receive granular data on energy usage. Use this data to identify inefficiencies and areas for improvement down to the room level, which can lead to significant cost savings over time.

Track the energy vitals of your facilities

When the energy consumption approaches or exceeds the baseline or historical average, notifications trigger to the selected users. OBEM notifies users are of any energy leakages to help them to take corrective actions.

Use configurable thresholds for both approaching or exceeding the baseline and historical average for each commodity.

Charts show you a visual indication through icons and tool tips when the consumption is approaching or has exceeded the threshold.

Continuous analysis of meter data

Meter faults include comparison options for baseline, fixed value, previous period, and last year.
  • High energy consumption
  • High occupied energy consumption
  • High unoccupied energy consumption
  • High weekend energy consumption
  • Electrical peak demand above threshold
  • Unoccupied peak demand above threshold
  • Weekend electrical peak demand above threshold
  • Meter flatline value detection
  • Meter offline detection

Create virtual meters

Use Net Zero Advisor Plus with limited metering infrastructure to create, track, and act on high value measurements.

Create virtual meters to substitute sub-metering or create calculated values online.

Configurable dashboards

Build new dashboards using available data from meters, global points, and virtual calculations. Use the drag and drop functionality to configure unique analysis and share saved values with colleagues and teams.

Meter spike detection and clean up

Meter data anomaly detection identifies extreme values and replaces erroneous data automatically.

Flexible Meter Tagging

Tag with unique identifier to help build reports and monitor patterns across energy use.