Net Zero Advisor - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Product Bulletin
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

The Net Zero Advisor package helps the user to streamline management of carbon reduction, energy use, and utility spend with easy-to-use software and support services that improve understanding, tracking, and reporting.

Gather
  • Consolidate siloed data automatically
  • Gathers utility bill data from multiple providers and consolidates the data in a single dashboard
  • Eliminate manual processing of data from disparate sources
  • Ensure information accuracy by directly importing provider data
  • Reduce data complexity with automated fault work orders
  • Ease the process to plan for achievable reduction targets and distribute accountability for goals to each location across your portfolio
Track
  • Track data across buildings to assist with reduction measures
  • Make informed decisions on how to reduce energy consumption and emissions across your buildings portfolio
  • Understand emissions with deeper insights into the sources​
  • Make informed energy reduction decisions across buildings​
  • Predict future energy use for budgeting and planning
  • Identify anomalies to recognize energy waste patterns
  • Reduce the manual burden of tracking goal progress and deviations
  • Use internal or external efficiency and carbon benchmarks to identify savings and areas to focus on
  • Observe savings over time in comparison to baselines
Report
  • Communicate the progress of energy and emissions programs, internally and externally
  • Facilitate accurate compliance statements and disclosure requirements
  • Ease the burden of meeting compliance and disclosure requirements
  • Reduce the time required for report development ​
  • Improve the credibility and reporting accuracy of KPIs
  • Identify and focus on areas with the highest improvement impact
  • Improve brand reputation by demonstrating environmental, social, and governance (ESG) leadership
Getting started is easy
  • No hardware required​
  • No building network connection needed​
  • No site survey​
  • Remotely configured​
  • Includes training and a handover
  • Uses the existing utility provider’s portal credentials or access to utility bills
From the Sustainability Manager tab, users can access the following features that display information based on utility bill data rather than onsite meters:
  • Net Zero Advisor
  • Goals and Targets
  • Energy Manager

Reports

The following reports are available with Net Zero Advisor:
  • Utility Bill Comparison: This report helps you to compare the spend appearing in multiple invoices, for the accounts under the selected building. The cost comparison and percentage deviation shown for a monthly or yearly basis, helping you to keep track of the utility spend and analyze it for an improving and deteriorating trend.
  • Energy Comparison by Location: This report compares the Consumption and Max Demand of different spaces for the same period. There is a data normalization feature along with the normal comparison which, when selected, eliminates the effect of weather. For example, if a Building Owner wants to compare the consumption or demand of Floor 1 and Floor 2 that are leased to the same company, the Owner can use this report to view the two floors that were responsible for the max demand that resulted in a penalty.
  • Energy Baseline By Space: This report displays the energy consumption against a baseline for spaces. View the actual consumption for the selected period, the baseline for the selected period, the change in consumption, and the percentage change with respect to the baseline.