Utility Bill Manager - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

Utility Bill Manager helps you to keep track of your financial spending, so you can understand your current return on investment (ROI) and savings.

The following additional features are discussed in further detail in the Overview of Utility Bill Manager:

  • Utility Bill Manager
  • Financial Spend
Note: From a manual entry perspective, the Utility Bill Manager feature is available with the base OBEM Energy package. To automate the entry of this information, an automated utility service is available, that requires the purchase of an additional license.