The Goals & Targets feature helps you to set long term goals for emissions
and energy reductions. Use the easy-to-use set up wizard to do the following tasks:
- Define your reduction goals. Create goals for carbon emission, emission intensity, energy consumption, and energy intensity.
- Set goals and targets at portfolio level and drill down to the building level.
- Receive automated recommendations for location and building level goals depending on the baseline year values and target year values.
- Customize goals for particular locations, buildings, and commodities.
After you set a corporate goal and assign location targets, you can set building targets. You can then track your progress on the Goals & Targets dashboard. The dashboard includes the following benefits:
- Create and track multiple goals in the intuitive user interface.
- Link goals together to view the vision for an entire organization in one place.
- Assess any deviation from the net zero goal and view the action required to maintain your goal.
After you set building targets, you have the option to add sub-targets to a goal. You can assign percentage reduction values to individual commodities to help you achieve your goal.
The Goals & Targets dashboard also has the option to view goal progress over a longer period using the at a glance view.
Use the At a Glance pane to do the following tasks:
- View goals in terms of carbon emission or energy consumption.
- View extrapolated carbon emission based on the historical year's emission.
- Change the portfolio emission to view a breakdown by location, and to view detailed contributions from each location.
- Receive guidelines for the reduction needed each year to achieve set goals.
- Compare baseline year and planned reduction each year against the actual and extrapolated emissions.
You can delete goals and sub-targets for better tracking of emissions and energy objectives to reflect changing regulations and reporting requirements.