Data sources - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

The data sources tab allows data to be fetched from the following communication protocols:

  • Microsoft SQL Server - Metasys ADS/ADX
  • BACnet – BACnet IP

When you configure the data source, you can discover devices and points, fetch historic data for selected points, Metasys Historian database only, setpoint attributes, and connect with the platform.