Dashboard builder - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

Based on your individual needs, you can configure dashboards using the Define Dashboard feature in Asset Manager and Energy Manager to display data for space, meters, or equipment. Select a chart and add the points that you need to display. You can share custom dashboard widgets, add comments on widgets, create multiple tabs under define dashboard to accommodate more custom widgets, and rearrange different tabs that have the custom widgets in any order.

The following custom dashboards are available:

  • Real-time table: Map up to 20 different points to view real-time data for binary, multi-state, and noncumulative analog points in a tabular form. The table displays the point name, template name, value, and last updated time. You can create up to five widgets for each page on the define dashboard.
  • Line chart: Map different points with the same unit of measure, or up to four different units of measure in the same chart.
  • Pie chart: Use a pie chart to see the contribution of the consumption of four buildings, in percentage, for that location. The contribution from each building shows in a percentage, providing an easy view to you as to which building is contributing the most in consumption.
  • Column chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Area chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Bar chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Heat map chart: Use a heat map for easy detection of hot spots that lead to high consumption and demand during different parts of the day. Use this data to make quicker corrective actions for when the hot spots occur. You can map a single point at a time. The minimum and maximum color range automatically fill, and you can edit these values.
  • Stacked column chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Column Line Chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Column Area Chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Stacked bar chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Stacked column aggregation chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Stacked column aggregation line chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Stacked column aggregation area chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Stacked column stacked area chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.
  • Scatter Chart: Map different points with the same units of measure, or up to four different units of measure in the same chart.