Metasys Integration through APIs - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

OBEM receives Metasys data, for Metasys 11.0 and later, through APIs. The OBEM data collection device UI includes an additional source called Metasys API. Device and point grid automatically gets filtered when selecting Metasys API. The API supports command and control from OBEM to controller points in Metasys.