EasyIO Integration - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12
Use the OBEM integration with EasyIO to perform the following tasks:
  • Authorize and authenticate the EasyIO controller from the broker to OBEM.
  • Enable OBEM auto configuration using OBEM auto configurator due to the standardization of the tree structure on the EasyIO controller
  • Publish and subscribe objects to read and write EasyIO objects from the OBEM dashboard.