Use the OBEM integration with EasyIO to
perform the following tasks:
- Authorize and authenticate the EasyIO controller from the broker to OBEM.
- Enable OBEM auto configuration using OBEM auto configurator due to the standardization of the tree structure on the EasyIO controller
- Publish and subscribe objects to read and write EasyIO objects from the OBEM dashboard.