Auto Configurator - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

The OpenBlue Auto Configurator (OBAC) is a cloud-based tool that integrates with the OBEM application. OBAC and OBEM use shared APIs to automate the configuration of projects and equipment points in OBEM. The auto configurator is capable of onboarding a site of 5000 points in 24 to 30 hours, creating and configuring equipment by utilizing controller and point hierarchy of the Metasys DB export file, and easy equipment-to-equipment relationship mapping. It is a rich source of built-in filter expression library for quick start configuration and onboarding process reducing the turnaround time directly impacting the time to revenue.