Arcadia Utility Cloud API Integration - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.7

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.7
Revision date
2024-02-12

OBEM can integrate with Arcadia’s Utility Cloud API to reliably automate the transfer of billing data, reduce manual effort, eliminate errors in data entry, and streamline analysis of utility consumption and costs. OBEM successfully connects to the utility bill data platform through API with less than 2% failure rate. The API integration reduces the time spent on data entry and data-related errors. The system logs are accurate and easily accessible for auditing purposes.

By integrating with the utility bill data platform, OBEM provides a more automated and efficient service but ensures that users have the most accurate and current data at their disposal. This helps with informed decision making and could lead to significant cost savings for the user.