Work Order Manager - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.2.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.2.1
Revision date
2022-11-14

These are provided based on requirement. The equipment name with serving space along with the fault data is made available through API for the third-party CMMS systems to consume and create work orders.

These valuable data from the building is useful for technicians in order to understand the cause of the fault, and to come prepare appropriately looking at the diagnostic data provided from OBEM.

The CMMS completes the loop by sending the data back to OBEM when the work order has been closed in the CMMS.