The OBEM Fault monetization feature calculates excess energy wastage during equipment fault condition. Fault monetization helps identify the critical energy drain in buildings, and helps with the prioritization of maintenance work. Energy wastage is calculated in electrical and thermal formats.
Monetization equations can be written using:
- Equipment data point
- Equipment specification
- Constants
Monetization equations work independent of read frequency, and algorithms automatically detect data point frequency and adjust calculation.