Support for custom units - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.2.1

OpenBlue Enterprise Manager Product Bulletin

Brand
Johnson Controls
Product name
OpenBlue Enterprise Manager
Document type
Product Bulletin
Document number
LIT-12012497
Version
4.2.1
Revision date
2022-11-14
Language
English

OBEM supports custom units using offline and virtual meters.

This feature helps users to create unique KPIs such as kWh/Occupant Count to measure the amount of electricity per occupant or other creative KPI.

Additionally, to enable such use cases, the offline meters support entered values to represent a count, state, or limit.

The data with custom units is available at the respective meter level dashboards and custom dashboards.