Use the Space Performance app to understand the spaces that are getting over utilized and underutilized. View trends of these spaces, and correlate between space utilization and occupant comfort, which requires the OpenBlue Companion app, to determine if the spaces that are underutilized have hot or cold calls causing discomfort to the occupants.
The following additional features are discussed in further detail in the
Overview of Space Performance:
- Space performance widgets
- Meeting effectiveness
- Heat maps