Measuring the indoor air quality (IAQ) is vital in ensuring that the occupants in a building are healthy and productive. OBEM introduces widgets that measure indoor air quality parameters like temperature, humidity and carbon dioxide. Each of these parameters are measured during the occupied schedule of the building as well as when the building is unoccupied to give the right picture to ensure that occupants are healthy and productive.
Use the top thermal deviations dashboards as a starting point to focus on top deviations of IAQ and point to the equipment directly conditioning the spaces.
View an overview of spaces where the IAQ is not maintained by policy and the associated equipment, and navigate to the equipment to understand the cause of this deviation.