Data sources - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.2.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.2.1
Revision date
2022-11-14

The data sources tab allows data to be fetched from different communication protocols, including the following:

  • Microsoft SQL Server - Metasys ADS/ADX
  • BACnet – BACnet IP

When the data source is configured, the system allows you to discover devices and points, fetch historic data for selected points (Metasys Historian database only), set point attributes, and connect with the platform.