Spaces - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Product Bulletin
Document number
LIT-12012497
Version
4.1
Revision date
2022-05-23

The Space Tree feature allows you to create a space hierarchy reflecting actual physical locations in the portfolio, including the following:

  • Portfolio
  • Location
  • Building

Space re-ordering allows the admin to setup the space hierarchy to reflect how the user wishes to view the spaces.

You have the flexibility to add spaces, for example, floor, wing and rooms below the building level. Each one can be named for customers’ requirements to provide ultimate flexibility.

The accurate creation of the space tree is critical to the functioning of the EM system. Setting up the tree to exactly mirror the physical portfolio allows the energy analysis to be accurate and precise.