Weather normalization - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.1
Revision date
2022-05-23

The Weather Normalization feature normalizes the consumption information by utilizing degree days, accounting for large swings in weather that might impact a building’s energy usage.

Degree days can be configured to account for the average consumption of a specific day based on the weather conditions. Average energy consumption can then be viewed based on the weather conditions. The EM application displays this data in a chart format, making it easier to analyze the information.