Support for custom units - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.1
Revision date
2022-05-23

EM supports custom units using offline and virtual meters.

This feature helps users to create unique KPIs such as kWh/Occupant Count to measure the amount of electricity per occupant or other creative KPI.

Additionally, to enable such use cases, the offline meters support entered values to represent a count, state, limit, etc.

The data with custom units is available at the respective meter level dashboards and custom dashboards.