Energy summary of commodities - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.1
Revision date
2022-05-23

The Energy Manager section of EM uses information from the building automation system to monitor consumption of various commodities mapped for that space.

Energy KPIs depict Energy consumption details for electricity, thermal, and water, such as EUI, consumption, and per capita consumption.

KPI Cards help you to briefly monitor the spaces and visualize the KPI Cards at Portfolio, Location, and Building levels. You can also view the Energy Savings against the baseline for each of the commodities, and the Carbon footprint corresponding with the current level of consumption.

KPI Cards also help you to easily view commodity consumption changes with respect to the baseline from the previous year and the locations and buildings that have contributed to an increase or decrease in EUI.