Energy density dashboards - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Product Bulletin
Document number
LIT-12012497
Version
4.1
Revision date
2022-05-23

Use EM dashboards to comprehend energy data intuitively. The information displayed identifies inefficiencies in building operation to help reduce energy costs.

The dashboards are user-friendly. The data on the dashboards is organized to easily navigate through your portfolio and quickly prioritize the facilities that need attention. All data from dashboards can be exported and used for further reference and analysis or appended with a report.

EM has built-in reporting templates that captures essential data at a periodic basis and makes it easy to distribute these reports to the stakeholders. The reports and dashboards are also useful to track and report regulatory reporting and emissions.