You can add a Virtual Point under a particular equipment. If you have to define a Virtual Point for an equipment category, you can do the same in the Virtual Template Configuration tab in the equipment configuration section in Setup.
You can use mathematical and logical function to combine two or more points from a template of the chosen equipment and define a Virtual Point.
These defined Virtual Points can be used in defining the FDD rules, and you can also use these points in Define Dashboard.