Indoor Air Quality Dashboards - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.1
Revision date
2022-05-23

Measuring the indoor air quality is vital in ensuring that the occupants in a building are healthy and productive. EM introduces widgets that measure indoor air quality parameters like temperature, humidity and carbon dioxide. Each of these parameters are measured during the occupied schedule of the building as well as when the building is unoccupied to give the right picture to ensure that occupants are healthy and productive.

Focus on top deviations of IAQ and point to the equipment directly which are conditioning the spaces by using the top thermal deviations dashboards as a starting point.

View an overview of spaces where the IAQ's is not maintained by policy and the associated equipment. Directly go to the equipment to understand the cause of this deviation.