Metasys Integration through APIs - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.1
Revision date
2022-05-23

EM receives Metasys data, for Metasys 11 and later, through APIs. The EM Data collector UI has an additional source called Metasys API. Device and point grid automatically gets filtered when selecting Metasys API. The API supports command and control from EM to controller points in Metasys.