EM receives Metasys data, for Metasys 11 and later, through APIs. The EM Data collector UI has an additional source called Metasys API. Device and point grid automatically gets filtered when selecting Metasys API. The API supports command and control from EM to controller points in Metasys.