Auto Configurator - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012497
Version
4.1
Revision date
2022-05-23

The OpenBlue Enterprise Manager Auto Configurator is a cloud-based tool that integrates with the EM application. Auto Configurator and EM use shared APIs to automate the configuration of projects and equipment points in EM. The auto configurator is capable of onboarding a site of 5000 points in 24 to 30 hours, creating and configuring equipment by utilizing controller and point hierarchy of the Metasys DB export file, and easy equipment-to-equipment relationship mapping. It is a rich source of built-in filter expression library for quick start configuration and onboarding process reducing the turnaround time directly impacting the time to revenue.