These are provided based on requirement. The equipment name with serving space along with the fault data is made available through API for the third-party CMMS systems to consume and create work orders.
These valuable data from the building is useful for technicians in order to understand the cause of the fault, and to come prepare appropriately looking at the diagnostic data provided from EM.
The CMMS completes the loop by sending the data back to EM when the work order has been closed in the CMMS.