Solar meter dashboards - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1.2

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Product Bulletin
Document number
LIT-12012497
Version
4.1.2
Revision date
2022-08-02

You can measure renewable energy generation through EM’s solar meter dashboards. Solar meter dashboards are available at the meter-level for the respective building to which the solar meter is tagged to. The Peak Solar Production dashboard helps you to track the solar generation peak, min, max, and average.

To track the saving impact of solar energy, you can create a virtual meter with point definition as Electricity KWH-Solar KWH. A net consumption chart is available at the virtual meter-level.