Meters and equipment - Johnson Controls - LIT-12012497 - Software Application - OpenBlue Enterprise Manager - 4.1.2

OpenBlue Enterprise Manager Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Product Bulletin
Document number
LIT-12012497
Version
4.1.2
Revision date
2022-08-02

You can add in Meters or Equipment points, including the following tasks:

  • Add and Edit the attributes of data source points
  • Historical Fetch and Sync
  • Create meters and submeters and map the points

Online and virtual meters are represented by unique icons that help you to distinguish different types of meters. Meters can include commodities such as electricity, natural gas, water, and steam. Offline meters, Virtual meters, and points can be added under the Meter configuration tab in the Setup. The offline data for the offline meters can be uploaded in the Offline points tab in the Mapped points section of the Setup. Equipment setup can include categories such as chillers, air handling units, boilers, pumps, and fans that can be monitored for performance.