The data sources tab allows data to be fetched from different communication protocols, including the following:
- Microsoft SQL Server - Metasys ADS/ADX
- BACnet – BACnet IP
When the data source is configured, the system allows you to discover devices and points, fetch historic data for selected points (Metasys Historian database only), set point attributes, and connect with the platform.