Configure OBEM to compare aggregate sub-meter data with data from the relevant main meter. This can help the manager identify faults and areas of high and low consumption.
To replicate this model, complete the following steps:
- Create online meters for the sub-meters in the building. In this example, there are eleven electrical sub-meters spread over three floors.
- Define the sub-meters to aggregate at the virtual meter. For example, the virtual meter SDB Total Meter collates the eleven sub-meters:
- Define the main physical meter without roll-up.