Johnson Controls setup check - Johnson Controls - LIT-12012563 - Software Application - OpenBlue Enterprise Manager - 4.0

OpenBlue Enterprise Manager Implementation Planning Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012563
Version
4.0
Revision date
2021-11-29

The team responsible for the installation must ensure that they have data points that work with OpenBlue Enterprise Manager.

Note: It is typical to set the sample interval to 15 minutes, or 900 seconds. This setting must match the OBEM setup to see data on the dashboards. In versions 1.1 and later, OBEM automatically detects the sample interval of a Johnson Controls system and adopts this sample interval for all points.