Compile a meter inventory with the following meter information. Information specific to electrical meters is in bold text:
- Meter name
- Module connected
- Commodity
- Load type
- Measurement units
- Scale of measurement
- Energy consumption
- Demand
- Power factor
- Apparent power
- Frequency
Meter serial numbers are not necessary, but it is useful to include them if you know what they are.
The following table is an example of a meter inventory matrix:
Meter | Location served by the meter | Description | Switchboard | Electrical chillers | House lighting & power, including car park and out door lighting |
---|---|---|---|---|---|
OBEM B4 01 | Basement 4 Store Room | Meter Supply to DBT--B4 (State Power) | MSB-1 (Part 2) | X | |
OBEM B4 02 | Basement 4 Store Room | Meters Supply to DBT--B4 | MSB-1 (Part 2) | ||
OBEM B3 01 | Tenant Electrical Riser | Meters Supply to House Services | MSB-1 (Part 1) | X | |
OBEM B3 02 | Basement 3 | Meters Supply to DBT-BL3 (State Power) | MSB-1 (Part 1) | X | |
OBEM L3 03 | Plant Room | Meters Supply to DBT-BL3 (ANZ Lighting) | MSB-3 |