Appendix B: Configuration checklist - Johnson Controls - LIT-12012563 - Software Application - OpenBlue Enterprise Manager - 4.0

OpenBlue Enterprise Manager Implementation Planning Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
Installation Guide
Document number
LIT-12012563
Version
4.0
Revision date
2021-11-29
Table 1. Configuration checklist
Configuration Enter values here Instructions
Hardware Data Collector
How many data collectors do you require?   Enter number of data collectors required (multiple isolated networks)
Specify the time zone for each data collector   Enter the time zone of each data collectors. If required.
List the locations and buildings that each data collector serves   Enter each locations for each data collector. If required.
OpenBlue Enterprise Manager Configuration - General
Schedule details for building level and subsequent levels   Provide building level schedules
Weekend and holiday details   Provide weekend and holiday schedules
Space Tree and Ontology
Spreadsheet containing the name of each location/campus/area. Is it defined in the Johnson Controls System Configuration Tool (SCT)?   Provide location/campus/area. Enter Yes or No if defined in SCT.
Spreadsheet containing the name of each location/building. Is it defined in the SCT?   Provide name of each location/building. Enter Yes or No if defined in SCT.
Spreadsheet containing the number of floors in each building. Is it defined in the SCT?   Provide number of floors in each building. Enter Yes or No if defined in SCT.
Gross area of each location, building, floor, wing, and room   Provide gross area of each location, building, floor, wing, and room.
Physical address of buildings   Provide address of each building.
Latitude and longitude of locations   Provide latitude and longitude of each location.
Floor information like name, wings, built-up area for floor and wing. Is this defined in the SCT?   Provide each floor information. Enter Yes or No if defined in SCT.
Space type defined as plant room or office area   Provide space type.