Software cloud specifications - Johnson Controls - LIT-12013739 - Software Application - OpenBlue Enterprise Manager - 4.4

OpenBlue Enterprise Manager Guide Specification

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
User Guide
Document number
LIT-12013739
Version
4.4
Revision date
2023-05-17

The software is built on the following:

  • Software as a Subscription (SaaS) – provided and activated through cloud-based licenses subscribed by the user in 1 or 3-year renewable options. Licenses support a flexible framework that provides the ability to buy license packages in units of Month. The following license packages are available:
    • OpenBlue Enterprise Manager (Energy)
    • OpenBlue Enterprise Manager (Operations)

Each of the packages contains three tiers that are tailored to the needs of the customer: Essential, Enhanced, Expert

  • Cloud solution: Microsoft Azure
  • Web Browser Support: Accessed using Google Chrome (v48 and above)
  • Backend: Microsoft .NET Core technology
  • Front End User Interface: built on rich user interface, namely HTML5 and AngularJS
  • Database: MS Azure SQL Server
  • Data Processing: HDInsight HBase (Hadoop)
  • Reporting Tools: HTML5 and Highcharts
  • Dashboards: HTML5, Highcharts, and AngularJS
  • Automated Email: Has the capacity to generate specific reports for configured data points and publish reports to a server folder or send them to a person or organization through email.